ACTION#.SOURCE

Description

This keyword defines the input source for an action.

Value Description
0 No source
1 Mains ready
2 Digital Input
3 Digital Dio (Bidirectional)
4 Actual Velocity
5 Axis Faulted
6 Home Complete
7 Motion Task in Position
8 Controlled Stop Active
9 Software Limit
10 Move Complete
11 Position Error, Absolute
12 Axis Enabled
13 Analog Input
14 Current Command
15 Velocity Error
16 Velocity Command
17 Position Feedback
18 Axis Disable Immediately
19 Brake State
20 Ready to Operate (RTO/BTB)

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 17

Default Value

0 (no source)

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen